To our valued customers: Please note that our warehouses and offices will be closed on Thursday, July 4th in observance of the holiday.
Same-Day Shipping in the next 3:14:08
Same-day shipping if you order in the next hours!
Need assistance? Call 1-800-715-4396
Industry News

Fairview Microwave Introduces New Waveguide-to-Coax Adapters with European IEC Standard Flanges

2/4/2021

New Flange-Style Waveguide-to-Coax Adapters Now In-Stock

Flange-Style Waveguide-to-Coax Adapters

IRVINE, Calif. - Fairview Microwave Inc., an Infinite Electronics brand and a leading provider of on-demand RF, microwave and millimeter wave components, has just launched a new line of euro-style flange, waveguide-to-coax adapters that are ideal for radar, satellite and wireless communications, and test instrumentation applications.

Fairview Microwave’s new waveguide-to-coax adapters cover a wide range of waveguide sizes that include European IEC standard flanges (including  UBR square cover, UDR and PDR types), WR-22 to WR-430, right-angle and end-launch coaxial connector options, and N-type, SMA, 2.92mm and 2.4mm connector choices.  

These new waveguide-to-coax adapters transform waveguide transmission lines into 50-ohm coaxial lines, which allows each adapter to cover the full frequency range of its waveguide band and power to be transmitted in either direction.

”Not only are these new flange-style waveguide-to-coax adapters compliant European IEC standards, they are ready and available off-the-shelf to address our customers’ urgent needs,” said Steven Pong, Product Line Manager, RF Passive Components.

Fairview Microwave’s new waveguide-to-coax adapters with IEC euro-style flanges are in-stock and available for immediate shipping.

For inquiries, Fairview Microwave can be contacted at +1-972-649-6678.

About Fairview Microwave:  
A leading supplier of on-demand RF and microwave products since 1992, Fairview Microwave offers immediate delivery of RF components including attenuators, adapters, coaxial cable assemblies, connectors, terminations and much more. All products are shipped same-day from the company’s ISO 9001:2015 certified production facilities in Lewisville, Texas. Fairview Microwave is an Infinite Electronics brand.

About Infinite Electronics:
Based in Irvine, Calif., Infinite Electronics offers a broad range of components, assemblies, and wired/wireless connectivity solutions, serving the aerospace/defense, industrial, government, consumer electronics, instrumentation, medical and telecommunications markets. Infinite’s brands include Pasternack, Fairview Microwave, L-com, MilesTek, Aiconics, KP Performance Antennas, PolyPhaser, Transtector, RadioWaves, ShowMeCables, INC Installs, Integra Optics and NavePoint. Infinite Electronics serves a global engineering customer base with deep technical expertise and support, with one of the broadest inventories of products available for immediate shipment.
###

Press Contact:
Peter McNeil
Fairview Microwave
17792 Fitch
Irvine, CA 92614
(978) 682-6936