To our valued customers: Please note that our warehouses and offices will be closed on Thursday, July 4th in observance of the holiday.
Same-Day Shipping in the next 3:14:08
Same-day shipping if you order in the next hours!
Need assistance? Call 1-800-715-4396

Tank Circuit Resonance Calculator

Fairview Microwave's Tank Circuit Resonance Calculator uses the simple formula (below) to calculate the system's resonant frequency.

Bookmark or "Favorite" this page by pressing CTRL + D.

Calculation

Note: SI prefixes are supported.
Ex: 10 nanoFarads = "10n", 15 microHenries = "15u", etc.

Result:

Resonant Frequency:

A tank circuit refers to an LC circuit in which the inductor (L) is placed in parallel with the capacitor (C). Tank circuits are especially useful due to their property of carrying resonance, and are implemented in several electrical applications, such as filters, frequency tuners, and oscillators.

PrefixSymbolValue
Tera'T'1012
Giga'G'109
Mega'M'106
kilo'k'103
PrefixSymbolValue
pico'p'10-12
nano'n'10-9
micro'u'10-6
milli'm'10-3