To our valued customers: Please note that our warehouses and offices will be closed on Thursday, July 4th in observance of the holiday.
Same-Day Shipping in the next 3:14:08
Same-day shipping if you order in the next hours!
Need assistance? Call 1-800-715-4396

Stripline Impedance Calculator

Fairview Microwave's Stripline Impedance Calculator uses the dimensions of the stripline, as well as the dielectric constant, to compute the characteristic impedance.

Bookmark or "Favorite" this stripline impedance calculator page by pressing CTRL + D.

Note: Units for width and height must be consistent

 
 
 
 
 
 
 

Result:

Impedance:

A stripline consists of a central conductor surrounded by dielectric material between two groundplanes. Striplines, in many cases, can be used where microstrips would be, so long as size is not a constraint. In fact, striplines often make components such as band-pass filter's more accurately, with more symmetric roll-off and no lower cutoff frequency.

PrefixSymbolValue
Tera'T'1012
Giga'G'109
Mega'M'106
kilo'k'103
PrefixSymbolValue
pico'p'10-12
nano'n'10-9
micro'u'10-6
milli'm'10-3