Same-Day Shipping in the next 3:14:08
Same-day shipping if you order in the next hours!
Need assistance? Call 1-800-715-4396
Industry News

Fairview Microwave Announces New Lines of Semi-Rigid Test Probes

2/18/2016

Semi-Rigid Test Probes from Fairview Allow Engineers to Quickly and Easily Test their Development Circuits

Semi-Rigid Test Probes Up to 6 GHz from Fairview Microwave

Allen, TX - Fairview Microwave Inc., a supplier of on-demand microwave and RF components, debuts a new family of semi-rigid test probes operating up to 6 GHz. Designed to assist in testing microwave circuits, these test probes are constructed of high quality semi-rigid coax and SMA Female connectors.

The new test probe assemblies from Fairview Microwave come in multiple cable diameters to help when attaching the unterminated end of the probe to a circuit board trace. There are two versions including straight-cut probe ends for those that would like to customize the dimensions of the center conductor and dielectric dimensions, as well as pre-stripped probe ends that are ready for immediate use. By soldering the outer conductor to the signal ground and the exposed center conductor to the trace carrying the signal of interest, simple sampling measurements can be made without having to create a separate subassembly circuit board or add a connector to the circuit layout which can take up valuable real estate.

Fairview provides 3 diameters of semi-rigid coax and 3 different lengths from 3 inches to 12 inches to fit a variety of trace widths and applications. All test probe cable assemblies are 100% RF tested to ensure the cable assemblies operate to 6 GHz and also to make sure that the SMA connector interface meets the 1.35:1 VSWR specification prior to shipping. To protect the small diameter coax from damage, each part is shipped in a clear protective tube that can also be used for storing the probes for future use. 

“Our new semi-rigid test probes provide engineers and designers a convenient, ready-to-use solution for testing their development circuits or troubleshooting and analyzing different portions of their circuits,” explains Brian McCutcheon, Vice President and General Manager at Fairview Microwave.

Fairview’s new semi-rigid test probe cable assemblies are now in-stock and available to ship today. You can view these new cables by visiting https://www.fairviewmicrowave.com/rf-products/semi-rigid-test-probes.html directly. Fairview Microwave can be contacted at +1-972-649-6678.

###

About Fairview Microwave

A leading supplier of on-demand RF and microwave products since 1992, Fairview Microwave offers immediate delivery of RF components including attenuators, adapters, coaxial cable assemblies, connectors, terminations and much more. All products are shipped same-day from the company’s ISO 9001:2008 certified production facilities in Allen, Texas.

Press Contact:

Brian McCutcheon
Fairview Microwave
1130 Junction Drive #100
Allen, Texas 75013
(972) 649-6678