Same-Day Shipping in the next 3:14:08
Same-day shipping if you order in the next hours!
Need assistance? Call 1-800-715-4396

RF Mixers

RF mixers from Fairview Microwave have SMA connectors, a minimum frequency range from 1 MHz to 2 GHZ and a maximum frequency of 1,000 MHz to 18 GHz depending on model. Fairview RF mixers have conversion loss is between 8 dB and 11 dB, LO to IF isolation is between 15 dB and 20 dB and RF to LO isolation is between 20 dB and 25 dB all of which is model specific. Power for these radio frequency mixers is between 7 dBm Watts and 10 dBm Watts.

Fairview RF mixers are in stock and ship worldwide the same day.