Same-Day Shipping in the next 3:14:08
Same-day shipping if you order in the next hours!
Need assistance? Call 1-800-715-4396

Reflection Attenuator Calculator

Fairview Microwave's Reflection Attenuator Calculator allows you to determine the two possible resistor values (R1 > Z0 & R1 < Z0) for a reflection attenuator (measured in Ohms).

Bookmark or "Favorite" this page by pressing CTRL + D.

Result:

R1 > Z0:
R1 < Z0:

Reflection Attenuators use two equal resistors, each grounded and connected to the same node, to attenuate a signal. For this reason, there are two possible solutions to the value of the resistors used, one larger than the system impedance and one smaller. Visit Fairview Microwave's RF coaxial attenuators page for product details.

PrefixSymbolValue
Tera'T'1012
Giga'G'109
Mega'M'106
kilo'k'103
PrefixSymbolValue
pico'p'10-12
nano'n'10-9
micro'u'10-6
milli'm'10-3