Related articles

Peter McNeil | May 16, 2024 | RF Terminations
A valuable tool for terminating any unused port or signal chain that may produce more energy than can be safely handled within the system is a high-power RF termination. RF terminations are used to absorb unwanted RF signal energy and convert that energy into heat. A key aspect of high-power RF terminations is the ability to absorb the energy directed to them with minimal reflections. With the rise of sub-6 GHz wireless applications, especially extended range communication and sensing, components such as high-power RF loads that operate to 6 GHz, are extremely useful in the laboratory and in the field.
There are many situations in communications and sensing applications where the RF energy from a transmitter needs to be stopped prior to other communication or sensing functions. This could be for radars with a switched front-end or for communication transmitters with a switched filter bank output. Other examples included when a communication or sensing circuit needs to go silent as quickly as possible or if a part fails and there is excess signal energy in the signal chain that needs to be safely dumped or it could damage other components. In the laboratory, there are many cases where a given signal path may need to be terminated while live during a test setup before being used, or the signal energy used in testing a device needs to be terminated when an output is switched. Some components and devices involved in high power signal chains may also need to be terminated with a high-power RF termination, such as directional couplers, circulators/isolators, hybris, signal generators, test transceivers, transmitters, etc.
This is why it is important for a high-power RF termination to be able to handle the sustained input power and peak input power while providing good VSWR across the frequency band of operation. For cellular systems, Satellite Communications (Satcom), distributed antenna systems (DAS), test/measurement, and radar, the common sub-6 GHz coaxial standards include DIN 7/16, 4.3-10, and N-type. Though there are other coaxial standards that operate in this frequency range and are commonly used for these applications, these coaxial standards are capable of carrying higher power levels and are more appropriate to high power RF terminations than an SMA, for example. Where a typical RF termination can handle a couple of watts of RF energy within the operation frequency range, high power RF terminations are typically designed to handle 5 Watts, 10 Watts, 50 Watts, or more.

Peter McNeil | Feb 15, 2024 | RF Terminations
At 26 GHz, there is substantial atmospheric absorption and much higher free space loss than at sub-6 GHz frequencies. Moreover, the interconnect such as 26 GHz attenuators and 26 GHz terminations, to drive a 26 GHz system intrinsically must be more compact than lower frequency interconnect, meaning that the power handling and loss of interconnect suitable for 26 GHz is greater than that of lower frequency interconnect.
26 GHz is a very active chunk of spectrum firmly in the millimeter-wave frequencies. As with many portions of the spectrum and RF components/devices/systems, 26 GHz doesn’t merely refer to the singular frequency of 26 GHz, but the spectrum around that frequency. For instance, there are automotive radar applications at 24 GHz to 24.25 GHz (an ISM band), which some 26 GHz hardware may be suitable for. There are also many other applications, such as Ultra-Wide Band (UWB) that operates from 21 GHz to 26 GHz, that could be considered part of the 26 GHz spectrum, Moreover, 24.25 GHz to 27.5 GHz marks the 5G n258 band (3GPP band n258). Hence, there are a variety of applications operating around 26 GHz where Attenuators and Terminations suitable for 26 GHz could be used.
This means that each individual transmission path at 26 GHz can carry much less signal energy and dissipates more signal energy than lower frequency transmission paths. This is why at 26 GHz, many applications use array antennas, otherwise known as advanced/active antenna systems (AAS). This means that many 26 GHz applications have many transmission paths to provide power and conditioned signals to array antennas, including phased array antennas. Depending on the architecture of the advanced/active array, there may be many transmission paths that require attenuation during testing or use, or terminations during testing/prototyping. This is where 26 GHz attenuators and 26 GHz terminations come into play. These components are vital for use during operation for AAS, but also during the development and testing phases. Attenuators are used to condition the power level of a signal during testing or use and increase the precision of a test by conditioning the output signal energy of a test signal source. Terminations are instrumental in providing impedance match loads at the end of a transmission path to prevent reflections. This is useful during calibration but also when a path may not be used and that signal energy needs to be shunted instead of reflected back to the source.