New Bandpass and Low Pass Filters Designed for Popular Frequency Bands
LEWISVILLE, Texas - Fairview Microwave Inc., a supplier of on-demand microwave and RF components, has introduced a new series of low pass and bandpass filters for use with multiple popular frequency bands.
Fairview’s 13 new SMA coaxial filters consist of seven bandpass filters and six low pass filters. The bandpass filters were developed for use in various applications including GPS, ISM, RFID and Wi-Fi systems and operate in several bands, some as low as 824 MHz and some as high as 5.875 GHz.
The new low pass filters allow for tailoring of the test setup for a specific application and support upper band edges of 100, 225, 400, 1000, 2000 and 3000 MHz. All of these new RF filters are available off-the-shelf and feature SMA female connectors.
“Often people have filters custom designed to fit their frequency plan. For some popular bands, this is not required. Additionally, when the schedule is critical, a filter that is close to your frequency plan may be good enough to meet the system requirements. Since our new filters can be shipped the same day, they can be life savers for your project,” said Mark Blackwood, Product Manager.
Fairview’s new low pass and bandpass SMA coaxial filters are in stock and ready for immediate shipment with no minimum order quantity. For detailed information on these products, please visit https://www.fairviewmicrowave.com/rf-products/low-pass-and-bandpass-sma-coaxial-filters.html.
For inquiries, Fairview can be contacted at +1-972-649-6678.