Fairview Microwave Releases New Waveguide Mixers, Detectors and Couplers
news release
New Line of High-Performance Waveguide Mixers, Detectors and Couplers
IRVINE, Calif. – Fairview Microwave, an Infinite Electronics brand and a leading provider of RF, microwave and millimeter-wave products, has just released a versatile selection of waveguide mixers, detectors and couplers. They address many applications, including 6G, 5G, research and development, test and measurement, electronic warfare and more.
The new couplers cover waveguide sizes ranging from WR-28 to WR-229. The integrated connectorized designs include 2.92 mm female, SMA and N-type connectors, plus coupling values from 20 to 50 dB
The waveguide detectors cover a frequency range from 26.5 GHz to 110 GHz. They are engineered with wide dynamic range from -55 dBm to +10 dBm, maximum input power of +17 dBm, and high levels of video sensitivity ranging from 750 mV/mW to 1500 mV/mW
Fairview Microwaves’ new waveguide mixers feature low conversion loss of from 8 to 12 dB with +13 dBm LO drive. Additionally, they cover broadband frequencies ranging from 26.5 to 110 GHz and LO-RF at 28 dB typical.
“Our customers will enjoy years of usefulness and best-in-class lead times with these new waveguide products. They ship from our ISO 9001:2015-certified facility and feature rugged designs constructed from the highest quality materials to stand up to years of use,” said Tim Galla, Product Line Manager.
About Fairview Microwave:
A leading supplier of on-demand RF and microwave products since 1992, Fairview Microwave offers immediate delivery of RF components including attenuators, adapters, coaxial cable assemblies, connectors, terminations and much more. All products are shipped same-day from the company’s ISO 9001:2015 certified production facilities in Lewisville, Texas. Fairview Microwave is an Infinite Electronics brand.
About Infinite Electronics:
Based in Irvine, Calif., Infinite Electronics is a global electronics supplier, offering a broad range of components, assemblies and wired/wireless connectivity solutions, serving the aerospace/defense, industrial, government, consumer electronics, instrumentation, medical and telecommunications markets. Infinite’s brands include Pasternack, Fairview Microwave, L-com, MilesTek, ShowMeCables, NavePoint, INC Installs, Integra Optics, PolyPhaser, Transtector, KP Performance Antennas, RadioWaves and Aiconics. Infinite Electronics serves their customer base with deep technical expertise and support, with one of the broadest inventories of products available for immediate shipment, fulfilling unplanned demand for engineers and technical buyers. Infinite Electronics is a Warburg Pincus portfolio company.
###
Press Contact:
Peter McNeil
Fairview Microwave
17792 Fitch
Irvine, CA 92614
(978) 682-6936