A Microstrip is a type of electrical transmission line used to transmit RF signals and are commonly fabricated using printed circuit board (PCB) technology. Compared to waveguides, microstrip is generally has a lower power handling capacity, and higher losses due to the fact that it is not enclosed.
**Note: Like our microstrip line impedance calculator, all of our RF calculators allow SI prefix input. For example, if you wish to input "25000000", just type "25M" instead. See the quick-reference table below for all compatible SI prefixes.